Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
Is there any problem if the core especially the upper yoke has a temperature of 120°C even on an idle run in Resiglas dry type transformers?
No,there is no problem if the core especially the upper yoke has a temperature of 120°C even on an idle run in Resiglas dry type transformers .It can even have temperature greater than 120˘C. The maximum permissible temperature of the core is defined only by the temperature withstand parameters of other parts of the transformer. Standard temperature protection for windings (class F) is set on 145° for alarm and 155°C for tripping.

Schneider Electric Egypt and North East Africa

Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more