{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Where to reconfigure, in BLAT, the SMTP server parameter
Issue
BLAT is configured on server to send out email using the Launching Module in VIP. The SMTP server has changed and need to reconfigure in BLAT.

Product Line
SPM7.x
PME7.x
Power Monitoring Expert (PME 8.x)

Environment
Windows

Cause
BLAT is configured on server to send out emails using the Launching Module in VIP. The SMTP server has changed and need to reconfigure BLAT

Resolution
When BLAT was configured on the server the install command only stores the various parameters in the Windows Registry. To change or verify the SMTP settings navigate to Regedit ->HKEY_LOCAL_MACHINE ->SOFTWARE ->Wow6432Node ->Public Domain ->Blat. The configured parameters that BLAT uses can be found here.

Schneider Electric Egypt and North East Africa

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: