{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Does the Modicon M580 support the use of Quantum ERIO drops?
Issue
Modicon M580 support for Quantum ERIO drops

Product Line
Modicon M580 PAC, Quantum

Resolution
The Modicon M580 models BMEx584040, 5040 and 6040 will support Quantum ERIO drops when used with Unity 11.0 running Hot Fix 1 or later. Hot Fix 1 will also allow State RAM addressing for the Quantum ERIO drop.

Schneider Electric Egypt and North East Africa