{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How do I lock out a switch based on a condition?
Issue:
Looking for a way to prevent or lock out a switch with a PLC status bit.

Product Line:
Vijeo Designer (all versions)

Resolution:
In Vijeo Designer, the switch object has an Interlock property that can be set with a specific condition. Until the condition is true, the switch will not execute its defined operation.

To configure the switch, double click on it to bring up the Switch Settings dialog.

1) Click on the Advanced Tab
2) Check the "Enable Interlock" checkbox
3) In the field, either create an expression or assign a BOOL variable.
4) Press OK.

Now the switch is deactivated until the condition or BOOL variable is true.

Schneider Electric Egypt and North East Africa