{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Are power boards on the ATV61 interchangeable on the ATV71 of the same frame size?
Issue:
Interchangeable power boards between ATV61 and ATV71 with same frame size.

Product Line:
Altivar 61 & Altivar 71

Environment:
All VFD of the same frame size with different horse power

Cause:
N/A

Resolution:
The Power boards are not interchangeable on the ATV61 or the ATV71 of the same frame size. Although the power boards are the same physical size based on frame size, some components on the power board are specific to the horse power and voltage rating.

Schneider Electric Egypt and North East Africa