{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can AR8008BLK or AR8016ABLK be used in the NetShelter Networking cabinets?
Issue:
The NetShelter SX Networking cabinets have open mounting rails which do not support the cable side channels.

Product Line:
NetShelter SX Networking

Environment:
All versions and serial ranges.

Cause:
A customer needs to run cables from front to rear in a NetShelter SX Networking cabinet.

Resolution:
In the Networking cabinets horizontal cable managers can be used to connect the side channels from front to rear. A typical setup would be to have AR8603A or AR8428 installed on the front and rear mounting rails, and run AR8008BLK or AR8016ABLK between them.

Schneider Electric Egypt and North East Africa