Issue
Documentation window will not come up
Product Line
ProWORX 32
Resolution
The ProWORX 32 Documentation window is either minimized or hidden behind another window. Close down the ProWORX 32 software. Deleted the "layout.acf" and/or "layout3.acf" file(s) from the C:\Proworx\32 folder. This resets the ProWORX 32 windows to default. Relaunch the ProWORX 32 software and the Documentation window should now reappear.
Documentation window will not come up
Product Line
ProWORX 32
Resolution
The ProWORX 32 Documentation window is either minimized or hidden behind another window. Close down the ProWORX 32 software. Deleted the "layout.acf" and/or "layout3.acf" file(s) from the C:\Proworx\32 folder. This resets the ProWORX 32 windows to default. Relaunch the ProWORX 32 software and the Documentation window should now reappear.
Released for: Schneider Electric Egypt and North East Africa