{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
How do you set up a run permissive on the S-Flex or ATV212 drives?
Issue:
Setting up a run permissive on the S-Flex or ATV212 drives.

Product Line:
Altivar ATV212 and S-Flex

Environment:
All

Cause:
The ATV212 drive is not shutting down when they open the permissive input on R.

Resolution:
For an open type ATV212 -
Find F--- Extended menu and enter
Set F110 = 0 to remove the always active permissive
Set F112 = 1 to assign R logic input as permissive, active when high
Now when the R digital input drops out, the drive will stop outputting power and will display OFF.

For S-flex units -
The R input is factory set for the permissive function, as above.
For S-Flex without bypass, a permissive contact should be wired between P24 and R terminals, mounted on the DIN rail
For S-Flex with bypass, DIN terminals 1 - 2 and 2 - 3 have jumpers from the factory that are normally used for damper end switch or fire/freeze stat inputs.  If any of these is not being utilized, remove the jumper and add the permissive contact.
See attached files for generic schematics.

Schneider Electric Egypt and North East Africa

Attachment(s)
SFlex bypass.pdf [200.66 KB]
SFlex no bypass.pdf [115.23 KB]
How do you set up a run permissive on the S-Flex or ATV212 drives?
Issue:
Setting up a run permissive on the S-Flex or ATV212 drives. 

Product Line:
Altivar ATV212 and S-Flex

Environment:
All

Cause:
The ATV212 drive is not shutting down when they open the permissive input on R.

Resolution:
For an open type ATV212 -
Find F--- Extended menu and enter
Set F110 = 0 to remove the always active permissive
Set F112 = 1 to assign R logic input as permissive, active when high
Now when the R digital input drops out, the drive will stop outputting power and will display OFF.

For S-flex units -
The R input is factory set for the permissive function, as above.
For S-Flex without bypass, a permissive contact should be wired between P24 and R terminals, mounted on the DIN rail
For S-Flex with bypass, DIN terminals 1 - 2 and 2 - 3 have jumpers from the factory that are normally used for damper end switch or fire/freeze stat inputs.  If any of these is not being utilized, remove the jumper and add the permissive contact.
See attached files for generic schematics.

Schneider Electric Egypt and North East Africa

Attachment(s)
SFlex bypass.pdf [200.66 KB]
SFlex no bypass.pdf [115.23 KB]
Explore more
Range:
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
Explore more
Range:
move-arrow-top