{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How do I connect the RPO(Remote Power Off) function If using multiple CL-NA units?
RPO (Remote Power Off)  connection for multiple CL-unit installations

By default the unit comes with a shorting link connection if the RPO function is not being used.

If  planning to use multiple CL units with RPO functionality you need to remove the shorting link and daisy chain the terminals as shown here







As you can see the last device in the daisy chain will be connected to an external switch which has normally closed contacts

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: