{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Video: Configuring Current Parameters on Altivar 32 & Altivar 320 Drives
Issue:
How low can I set the amperage settings on the ATV32 and ATV320 drives?

Product Line:
ATV32, ATV320

Environment:
All serial numbers for ATV32 and ATV320

Resolution:
On the ATV32 and ATV320 drives, there are 3 amperage settings (nCr, iTH, and CLI)
nCr (Motor Rated Current) - 0.25 to 1.5 In (1) - According to drive rating and [Standard mot. freq] (bFr)
iTH (Motor Thermal Current) - 0.2 to 1.5 In (1) - According to drive rating
CLI (Current Limitation) - 0 to 1.5 In (1)

*In - Drive rated current


Schneider Electric Egypt and North East Africa