{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What faults are not protected by Fault Inhibition on the ATV61 drive?
Issue:
What faults are not protected by Fault Inhibition on the ATV61 drive?

Product line:
ATV61, altivar 61

Environment:
all

Cause:
Customer was using Fault Inhibition, but the drive still tripped on SCF5, motor short circuit.

Resolution:

The fault inhibition function will be able to inhibit (not display) the fault detection on the « software » fault.
For the critical, internal or hardware faults, the inhibition function does not work to protect the drive from damage.

The fault list given in the programming manual are the ones that Inhibition will work
  • EnF, InFA, InFb, SOF, SPF, and tnF, APF, CnF, COF, EPF1, EPF2, FCF2, Fd1, LFF2, LFF3, LFF4, nFF, ObF, OHF, OLC, OLF, OPF1, OPF2, OSF, OtF1, OtF2, OtFL, PHF, PtF1, PtF2, PtFL, SLF1, SLF2, SLF3, SPIF, SSF, tJF, ULF and USF  faults can be inhibited and cleared remotely by means of a logic input or control bit ([Fault inhibit assign.] (InH) parameter

All the other critical, internal and hardware faults (SCFx, ILx, INFE, CRFx...) will be always active even with INH (fault inhibition) turned on.

Schneider Electric Egypt and North East Africa

What faults are not protected by Fault Inhibition on the ATV61 drive?
Issue:
What faults are not protected by Fault Inhibition on the ATV61 drive?

Product line:
ATV61, altivar 61

Environment:
all

Cause:
Customer was using Fault Inhibition, but the drive still tripped on SCF5, motor short circuit. 

Resolution:

The fault inhibition function will be able to inhibit (not display) the fault detection on the « software » fault.
For the critical, internal or hardware faults, the inhibition function does not work to protect the drive from damage.
 
The fault list given in the programming manual are the ones that Inhibition will work
  • EnF, InFA, InFb, SOF, SPF, and tnF, APF, CnF, COF, EPF1, EPF2, FCF2, Fd1, LFF2, LFF3, LFF4, nFF, ObF, OHF, OLC, OLF, OPF1, OPF2, OSF, OtF1, OtF2, OtFL, PHF, PtF1, PtF2, PtFL, SLF1, SLF2, SLF3, SPIF, SSF, tJF, ULF and USF  faults can be inhibited and cleared remotely by means of a logic input or control bit ([Fault inhibit assign.] (InH) parameter
 
All the other critical, internal and hardware faults (SCFx, ILx, INFE, CRFx...) will be always active even with INH (fault inhibition) turned on.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
Explore more
Range:
move-arrow-top