{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

How to Program If-Then-Else Statements in SCADAPack Workbench FBD Language

SCADAPack Workbench supports four standard IEC 61131-3 programming languages for CAM5 and three standard IEC 61131-3 programming languages for CAM3. These languages can be mixed within an application to provide an optimum control strategy.

Typically If-Then-Else Statements are best used with Structured Text Language (ST). In some instances, it may be desired to use these types of statements in a Function Block Diagram (FBD). Although not as elegant as ST, this can be achieved with JUMP's and LABELS in a FBD program.

The below example shows how to create an If-Then_Else statement in both FBD and ST.

image

image2

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: