{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How can I prevent Undervoltage faults on ATV61 drives?
Issue:
Prevent Undervoltage fault on ATV61 drive.

Product line:
ATV61, Altivar 61, ATV71, Altivar 71

Environment:
All

Cause:
Temporary voltage drops is causing UVR - Under voltage fault

Resolution:
Go to Drive Menu > 1.8 Fault Management > Undervoltage Mgt, and change the Undervoltage timeout from 0.2s to somewhere between 5-10s.

If the line voltage is less than 480VAC, we can also look at adjusting the Mains Voltage setting to 460V which lowers the trip level for the Undervoltage fault.

Schneider Electric Egypt and North East Africa