{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can the PT windings' polarities be swapped without affecting the measurements ?

Issue
Both the primary and the secondary PTs have been reversed for ease of installations in some cases as shown below.

Normal PT setup Both of PTs primary and secondary sides are reversed
Normal PT Setup Primary and Secondary PT's reversed

Product Line
All Powerlogic devices that need a set of PTs

Resolution
Swapping the polarity at both the primary and secondary sides of the PT as shown in above diagram cancels the effect - the signal will not be inverted and the meter should be able to monitor the system as designed.  However, if only one of the sides is swapped, the signal will be inverted and the meter might not read the correct voltage values.

Schneider Electric Egypt and North East Africa