Search FAQs
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
Compatibility & Inter-Operability between Vijeo citect, Vijeo Historian, Ampla and windows O.S and Office platforms and connectors.
Check attached PDF for compatibility and inter-operability.
Compatibility Matrix
1 Vijeo Citect V7.30 Service Pack 1 is the minimum requirement to be compatible with Windows 8 and Windows Server 2012. Windows 8.1 is not confirmed at this time.
5 Vijeo Citect V7.20 Service Pack 5 is the minimum requirement to be compatible with Windows 8.1 and Windows Server 2012 R2.
3 Vijeo Citect V7.10 Service Pack 3 is the minimum requirement to be compatible with Windows 7.
+ Not supported as a database for Inventory. Other modules are supported.
^ Windows 8.1 is not confirmed at this time
# Ampla supports the operating system on the client side only.
♦ Ampla 2014 and 2013 Server is compatible with the 64 bit version only. The client supports 32 and 64 bit.
Software is compatible with the 32 bit version only
▶ Server only
∞ Client only
Inter-operability
*Software is installed as part of PlantStruxure PES suite # Software is compatible via an OPC DA Connector only
Compatibility Matrix
1 Vijeo Citect V7.30 Service Pack 1 is the minimum requirement to be compatible with Windows 8 and Windows Server 2012. Windows 8.1 is not confirmed at this time.
5 Vijeo Citect V7.20 Service Pack 5 is the minimum requirement to be compatible with Windows 8.1 and Windows Server 2012 R2.
3 Vijeo Citect V7.10 Service Pack 3 is the minimum requirement to be compatible with Windows 7.
+ Not supported as a database for Inventory. Other modules are supported.
^ Windows 8.1 is not confirmed at this time
# Ampla supports the operating system on the client side only.
♦ Ampla 2014 and 2013 Server is compatible with the 64 bit version only. The client supports 32 and 64 bit.
Software is compatible with the 32 bit version only
▶ Server only
∞ Client only
Inter-operability
*Software is installed as part of PlantStruxure PES suite # Software is compatible via an OPC DA Connector only
Released for:Schneider Electric Egypt and North East Africa
Attachment(s)
Explore more
Range:
Explore more
Range: