Issue:
Minimum speed the VFD can safely operate a motor?
Product Line:
ATV212, ATV21, ATV312, ATV12, ATV32, ATV66, ATV71, ATV61, ATV11, ATV58, ATV31
Environment:
All serial numbers
Cause:
N/A
Resolution:
The VFD can safely run to a motor to 0.01 hertz, however, the lowest speed is dependent on what the motor/application can handle.
Minimum speed the VFD can safely operate a motor?
Product Line:
ATV212, ATV21, ATV312, ATV12, ATV32, ATV66, ATV71, ATV61, ATV11, ATV58, ATV31
Environment:
All serial numbers
Cause:
N/A
Resolution:
The VFD can safely run to a motor to 0.01 hertz, however, the lowest speed is dependent on what the motor/application can handle.
Released for:Schneider Electric Egypt and North East Africa