{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
Unexpected number of leak sensor detected alarm on an ACRC301X.
Issue:
Unexpected number of leak sensor detected alarm on an ACRC301X.

Product line:
ACRC301S, ACRC301H.

Environment:
All Serial Numbers.

Cause:
Install.

Resolution:

How to install the leak detection cable on an ACRC301X without getting an unexpected number of leak sensors detected.
Remove leak sensors from P510 and make sure they are the Netbotz Leak detection cable (NEBS0308). (Figure 1)
1
Figure 1


Through the display set the number of leak sensors to zero.
Path Configuration\Unit\Configuration\ Page 4 of 4
Attach leak sensor to the P510 port on the J5 controller.
Press the reset button on the J5 controller located just next to P513 (Figure 2 )

2
Figure 2

After reboot go into the display and change the number of leak sensors to read 1.
Path Configuration\Unit\Configuration\ Page 4 of 4
Test leak sensor.












Schneider Electric Egypt and North East Africa

Explore more
Range:
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
Product: