{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Setting Up GPRS Modem Diagnostic Session on SCADAPack E

Issue

Setting up GPRS communications can be very tricky, issue can be on modem side, mobile operator, SCADAPack and etc.

Product Line

SCADAPack E RTUs

Environment

E Configurator, Telnet

Resolution

SCADAPack E range has a very powerful diagnostic capabilities that allow to look at very deep level. To access it we will need Ethernet or Serial connection to RTU.

  • Configure the serial port to Command Line mode:
  • in case of Ethernet connection:
Launch any Telnet client. I will use Kitty
Specify the connection string:

Then we should be able to see SCADAPack Prompt:

There are many diagnostic services that are running on the SCADAPack E, in order to get only required information about GPRS connection we need to setup filters.
Type the following command tcpdiag Response will indicate current active filters:

We can disable all of them by typing tcpdiad disable *

After that we can specify the filters gprs and ppp by typing tcpdiag enable gprs ppp:


Then we will enter diagnostic monitor by issuing diag command:


We should be able to see the process of connection establishment, sending AT Initialisation string and network attachment:


And if the modem configured correctly we will see that modem will be assigned with IP address:

Schneider Electric Egypt and North East Africa

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.