{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is there any Ethernet/IP Client available in SoMachine or Machine Expert?
Starting with SoMachine  version 4.1 SP2, an EtherNet/IP Client device for TM251MESE controllers is available. TM251MESC controllers do not have this feature available in SoMachine or Machine Expert 1.2 or 2.x

Starting with SoMachine version 4.2, an Ethernet/IP Client device for TM241CE controllers is also available. TM241CEC** controllers do not have this feature available in SoMachine version 4.2 but starting with SoMachine version 4.3 it is is available.

All M262 controllers which were introduced with Machine Expert have the Ethernet/IP Client functionality.

Note: SoMachine software is now called Machine Expert. The last version of SoMachine was 4.3.

Schneider Electric Egypt and North East Africa