{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Can the ATV21, ATV212, or S-Flex drives communicate using Ethernet IP protocol?

Issue:
ATV21, ATV212, S-Flex drives network connection using Ethernet IP Communication

Product Line:
Altivar 21 / ATV21
Altivar 212 / ATV212
S-Flex enclosed drives

Resolution:
No.  These drives do not have the capability to connect directly to an Ethernet IP network.  A gateway is required to convert Ethernet IP to a standard protocol supported by the drive, such as Modbus RTU.

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:

Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: