This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
The rating for NG125NA is the same for both utilization categories AC22A/B and AC23.
Note: The utilization category impacts the electrical endurance and the making and breaking capacities according to IEC 60947-3 standard,as per the table in the attached guide page.
Note: The utilization category impacts the electrical endurance and the making and breaking capacities according to IEC 60947-3 standard,as per the table in the attached guide page.