Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
Can we adjust the voltage output of an Altivar to be reduced from 380 to 220 Volts?
As per the understanding, the line supply voltage will be 380V or 400V, and you want to set the output voltage to the motor to be 220 V.

Yes, It is possible. You can set the motor name plate voltage to 220V in setting menu or  Motor control (DRC) menu, so that the maximum output voltage will be capped at 220V. When you set the motor voltage to 220V in VFD, the VFD will not allow the output voltage more than 220VAC even though the input voltage is 400VAC.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range: