Issue:
Where can I find information on the 1.1 through 1.5 LED indicator lights?
Product Line:
ALTIVAR 61/71
Environment:
All
Cause:
Product Selection & Services
Resolution:
LED's 1.1-1.5 belong to Controller Inside Card (or similar, like a Water Solutions Pump Card).
When used with a Controller Inside Card (CIC), the LED's indicate status as shown below in an excerpt from the ATV61/71 Controller Inside manual:

When used with a Water Solutions Pump Card, the LED's indicate status as shown below in an excerpt from the Water Solution Control Card User manual:

For further details see the attached files.
Where can I find information on the 1.1 through 1.5 LED indicator lights?
Product Line:
ALTIVAR 61/71
Environment:
All
Cause:
Product Selection & Services
Resolution:
LED's 1.1-1.5 belong to Controller Inside Card (or similar, like a Water Solutions Pump Card).
When used with a Controller Inside Card (CIC), the LED's indicate status as shown below in an excerpt from the ATV61/71 Controller Inside manual:
When used with a Water Solutions Pump Card, the LED's indicate status as shown below in an excerpt from the Water Solution Control Card User manual:
For further details see the attached files.
Released for:Schneider Electric Egypt and North East Africa