{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is the OFS server designed only to run under the active users when it is running as process only.
Issue
Is the OFS server designed only to run under the active users when it is running as process only.

Product Line
OPC Factory Sercer (OFS)

Environment
Windows 10 version 1902, OFS v3.62

Resolution
OFS is configured through DCOM to run with the Interactive user identity, that is the logged user.

Schneider Electric Egypt and North East Africa