{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What can cause a CF12 fault [Download transfer fault] on an ATV212 drive?
Issue:
CF12 fault [Download transfer fault] on an ATV212 drive.

Environment:
All models and serial numbers

Cause:
The download transfer fault can be caused by parameter F807 not being set to 0.

Resolution:
Parameter F807 selects the communication channel.  The two choices are 0 [RJ45] and 1 [Open style].  The default setting is 1.  If SoMove or the IPAD app is being used to configure the drive parameter F807, then it must be set to 0.

Schneider Electric Egypt and North East Africa