Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
Which trip unit in MCCB achieve LSI protection
1-For Compact NSX: the required trip unit with adjustable Long time protection (L)and short time protection(S) with instantaneous protection (I) can be achieved with Micrologic 2 trip unit taking into consideration that the time delay for L and S functions is non-adjustable.

If these protection functions are required with adjustable time delay, you must opt to offer the Micrologic 5.

2-For Compact NS: the required protection functions LSI can be achieved with Micrologic 5 with time delay adjustable for long time and short time protection functions.

Schneider Electric Egypt and North East Africa

Attachment(s)
Compact NS micrologic 2.pdf [116.1 KB]
NSX micrologic 2.pdf [134.12 KB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range: