Search FAQs
What is the maximum motor distance for an Altivar 212?
Issue:
Maximum motor distance for an Altivar 212.
Product Line:
ATV212
Environment:
All serial numbers for ATV212
Cause:
N/A
Resolution:
The maximum motor cable length is 50m (164ft). This maximum can be increased with the use of a motor choke.
Maximum motor distance for an Altivar 212.
Product Line:
ATV212
Environment:
All serial numbers for ATV212
Cause:
N/A
Resolution:
The maximum motor cable length is 50m (164ft). This maximum can be increased with the use of a motor choke.
Released for:Schneider Electric Egypt and North East Africa
Explore more
Range:
Explore more
Range: