Search FAQs
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What is the Icw rating for Compact NSX MCCBs?
We have no Icw (rated short-time withstand current) values for the NSX up to 630A. These devices have an utilization category A according IEC 60947-2 standards which means that they are not specifically intended for selectivity under short-circuit conditions with respect to other short-circuit protective devices in series on the load side. And as per IEC 60947-2, Icw not required for the utilization category A MCCBs and it only exists for utilization category B circuit breakers.
Released for:Schneider Electric Egypt and North East Africa
Explore more
Range:
Explore more
Range: