Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
Are there different licenses for Vijeo Designer Runtime based on tag counts or number of tags used?
Issue:
Are there different licenses for Vijeo Designer Runtime based on tag counts or number of tags used?

Product Line:
Vijeo Designer Runtime Software
VJDSNRTMPC, VJDSNRTSPC

Environment:
HMI runtime software for Windows

Resolution:
Vijeo Designer Runtime is a single license that is not based on tag count or number of tags used.  The Runtime license is fully functional to all features in Vijeo Designer development as long as the hardware supports it.  The Vijeo Designer Runtime can run on the Harmony/Magelis Industrial PCs (iPCs) or a Standard Windows PC.

For Vijeo Designer v6.2 Service Pack 10 and older, the part numbers were (and are no longer commercialized):
VJDSNRTMPC  Runtime iPC
VJDSNRTSPC  Runtime Standard PC

For Vijeo Designer v6.2 Service Pack 11 and higher, the part numbers are:
VJDRPCCZLSPMZZ - Vijeo Designer Runtime, Standard PC & Harmony PC (except HMIBMP,HMIBMU,HMIPSO,HMIPSP,HMIPEP), printed
VJDRPCCZLSPAZZ - Vijeo Designer Runtime, Standard PC & Harmony PC (except HMIBMP,HMIBMU,HMIPSO,HMIPSP,HMIPEP), email
VJDHPCCZLSPMZZ - Vijeo Designer Runtime, Harmony PC ( HMIBMP,HMIBMU,HMIPSO,HMIPSP,HMIPEP)/Harmony P6, printed
VJDHPCCZLSPAZZ - Vijeo Designer Runtime, Harmony PC ( HMIBMP,HMIBMU,HMIPSO,HMIPSP,HMIPEP)/Harmony P6, email
 

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range: