Issue
Part number for programming cable
Product Line
TSX Momentum
Resolution
The part number for the TSX Momentum modbus programming cable is a 110XCA20300 (DB9 - RJ45 Adapter) and one of the below 110XCA2820X communication cable depending of length needed:
110XCA28201 RS232 Communication Cable—3ft, RJ45–RJ45.
110XCA28202 RS232 Communication Cable—10ft, RJ45–RJ45.
110XCA28203 RS232 Communication Cable—20ft, RJ45–RJ45.
Part number for programming cable
Product Line
TSX Momentum
Resolution
The part number for the TSX Momentum modbus programming cable is a 110XCA20300 (DB9 - RJ45 Adapter) and one of the below 110XCA2820X communication cable depending of length needed:
110XCA28201 RS232 Communication Cable—3ft, RJ45–RJ45.
110XCA28202 RS232 Communication Cable—10ft, RJ45–RJ45.
110XCA28203 RS232 Communication Cable—20ft, RJ45–RJ45.