Search FAQs
How does one change the direction of the drive in a S-FLEX Drive without affecting bypass?
Issue:
S-FLEX Drive direction modification without affecting bypass
Product Line:
Altivar 212, ATV21, S-Flex, SFLEX
Environment:
All
Cause:
Wrong rotation in drive and correct rotation in bypass
Resolution:
With power disconnected from the unit, swap 2 of the leads leaving the T1, T2, and T3 terminals on the ATV212 or any 2 connecting to the input side of the drive output contactor (DOC).
Do NOT swap phases at the incoming circuit breaker or at the motor connections on the Overload Relay.
This will ensure that the drive's rotations is changed but bypass will stay the same.
S-FLEX Drive direction modification without affecting bypass
Product Line:
Altivar 212, ATV21, S-Flex, SFLEX
Environment:
All
Cause:
Wrong rotation in drive and correct rotation in bypass
Resolution:
With power disconnected from the unit, swap 2 of the leads leaving the T1, T2, and T3 terminals on the ATV212 or any 2 connecting to the input side of the drive output contactor (DOC).
Do NOT swap phases at the incoming circuit breaker or at the motor connections on the Overload Relay.
This will ensure that the drive's rotations is changed but bypass will stay the same.
Released for:Schneider Electric Egypt and North East Africa
Explore more
Range:
Explore more
Range: