This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
We have not tested iC60/C60 for Icw test as per IEC 60947-2 standard. Icw (Rated short-time withstand current) tests are more dedicated to the switch-disconnector ranges (according to IEC60947-3) or Utilization Category B Circuit breakers