{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How long can the ATV630 or ATV650 motor leads be before I need an output filter?
Issue:
ATV630 and ATV650 motor leads maximum length before an output filter is required.

Product Line:
ATV630, ATV650 process drive.

Environment:
All models, All serial numbers

Cause:
Information needed to plan for installation

Resoultion:
Please see the chart below for the maximum distance of motor leads before output filtering is mandatory.   Note that the distances listed are the maximum distance before output filtering is required.  Output filtering may be necessary at shorter distances for your specific installation.

Schneider Electric Egypt and North East Africa

Attachment(s)
output filter requirements.pdf [59.36 KB]