Search FAQs
How do you set up the damper control on the enclosed S-Flex ATV212 Drive?
Issue:
Setting up the damper control on the enclosed S-Flex ATV212 Drive
Product Line:
S-Flex ATV212 with bypass
Environment:
All
Cause:
Wants to wire in a damper control circuit to allow the damper to open before running the motor thru the drive.
Resolution:
Step #1 Customer commands the drive to run by closing terminals (5-6) auto start. (Drive will not start at this time or until damper is opened)
Step #2 Closing the auto start terminals (5-6) will energize the RPR relay which will close user contacts (19-20) to start damper solenoid coil.
Step #3 Damper solenoid will start to open damper.
Step# 4 Once the damper is open the customer will need to provide a end of damper feedback limit switch.
Step #5 Remove the jumper from terminals (3-4) and wire your end of damper feedback dry NO contact to terminal (3-4).
Please note that this damper function will only work in the remote control mode by closing contacts (5-6) and not the local mode run button on the face of the drive.
Setting up the damper control on the enclosed S-Flex ATV212 Drive
Product Line:
S-Flex ATV212 with bypass
Environment:
All
Cause:
Wants to wire in a damper control circuit to allow the damper to open before running the motor thru the drive.
Resolution:
Step #1 Customer commands the drive to run by closing terminals (5-6) auto start. (Drive will not start at this time or until damper is opened)
Step #2 Closing the auto start terminals (5-6) will energize the RPR relay which will close user contacts (19-20) to start damper solenoid coil.
Step #3 Damper solenoid will start to open damper.
Step# 4 Once the damper is open the customer will need to provide a end of damper feedback limit switch.
Step #5 Remove the jumper from terminals (3-4) and wire your end of damper feedback dry NO contact to terminal (3-4).
Please note that this damper function will only work in the remote control mode by closing contacts (5-6) and not the local mode run button on the face of the drive.
Released for:Schneider Electric Egypt and North East Africa
Explore more
Product:
Range:
Explore more
Product:
Range: