Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
How do you create segment names in ProWORX 32?

Issue
Create segment names in ProWORX 32

Product Line
ProWORX 32

Resolution
To give names to Segments in ProWORX 32, you need to first open the Documentation window. Enter the Segment reference number. For example, Segment 1 would be S01. Segment 20 would be S20. The Segment name can then be entered as a Descriptor and will show up in the Network Navigator window as the title of the Segment number. The Segment name will show up once you put the cursor back in the logic window. See the attached screen shot as an example.

Schneider Electric Egypt and North East Africa

Attachment(s)
ProWORX 32 Creating Segment Name.pdf [292.09 KB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range: