{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
PowerChute Network Shutdown registers with Network Management Card during set up but after registering reports it cannot communicate with NMC.
Issue:
PowerChute Network Shutdown registers with Network Management Card during setup, but after registering reports, it cannot communicate with NMC.

When PowerChute registers with the Network Card, it expects to receive UDP packets from the card on port 3052. The error listed in the image below will be posted if the packets are not received.

Error message, Not receiving data from Network card

Product Line:
PowerChute Network Shutdown

Environment:
Windows OS with multiple NICs

Cause:
Windows firewall

Solution:
Follow the instruction in FAQ FA159624
If following the instruction in FAQ FA159624 did not resolve the issue the solution may be to add a new firewall rule that opens UDP port 3052 to all network profiles.
To add a firewall rule open a command prompt as an administrator and type
netsh advfirewall firewall add rule name="PCNS UDP port 3052" dir=in action=allow profile=any protocol=udp localport=3052

Schneider Electric Egypt and North East Africa

Explore more
Range:
Category:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
Category: