Search FAQs
How do we ACK alarms on an HMI from a PLC bit?
Issue:
Looking for a way to programmatically ACK alarm on the HMI from a PLC bit.
Product Line:
Vijeo Designer, Vijeo Designer Runtime
Resolution:
To allow a PLC bit to ACK all alarms displayed in the Alarm Summary, the following script call should be made in a Panel Action (on the same panel as the Alarm Summary).
<Alarm Group name>.ackAll();
Note: The action should be configured as Conditional and to execute when the PLC bit is "True".
The attached project makes use of a Panel Action that executes an AlarmGroup script when a PLC bit is "True".
Please see the attached project for the example.
Looking for a way to programmatically ACK alarm on the HMI from a PLC bit.
Product Line:
Vijeo Designer, Vijeo Designer Runtime
Resolution:
To allow a PLC bit to ACK all alarms displayed in the Alarm Summary, the following script call should be made in a Panel Action (on the same panel as the Alarm Summary).
<Alarm Group name>.ackAll();
Note: The action should be configured as Conditional and to execute when the PLC bit is "True".
The attached project makes use of a Panel Action that executes an AlarmGroup script when a PLC bit is "True".
Please see the attached project for the example.
Released for:Schneider Electric Egypt and North East Africa
Attachment(s)
Explore more
Range:
Explore more
Range: