{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What communication protocols are available on the Altivar 32?

Article available in these languages: Spanish

Issue:
Communication protocols available for the Altivar 32

Product line:
Altivar 32, ATV32

Environment:
all

Cause:
n/a

Resolution:

The Altivar 32 drive integrates Modbus and CANopen as standard communication protocols. Both can be accessed via the RJ45 connector on the front of the drive.
To simplify connection of the Altivar 32 drive to the CANopen machine bus, three communication card options are available with different connectors:
. CANopen daisy chain card with two RJ 45 connectors
. CANopen card with 9-way SUB-D connector
. CANopen card with 5-way terminal block

In addition to Modbus and CANopen as standard protocols, the Altivar 32 drive can be connected to industrial communication networks by adding one of the following
optional communication cards:
. Modbus/TCP - Ethernet/IP
. PROFIBUS DP V1
. DeviceNet
. EtherCAT

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: