Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
does we have Steel enclosure with sheet thickness 2mm ?
 We don't have in our offer the mentioned dimensions with thickness of sheet metal = 2 mm. Yet the IK, degree of protection =IK10 conforming to IEC 62262 (impact energy 20 J (40 cm , 5KG)).
So this guarantee the mechanical withstanding and we don't have any needs to have thickness = 2mm.

Schneider Electric Egypt and North East Africa

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.