{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How long are the data or application saved in the flash memory of a M340?
Issue
How long is the application or data stay in the Flash memory of a M340?

Product Line
M340

Resolution
Once data or application are stored on flash memory, no energy is needed anymore (same than your data on USB key, since all USB keys are made of Flash memory) => we consider 10 years, but this is an average value for Flash technology and it is more than enough for our controllers!

Schneider Electric Egypt and North East Africa