Search FAQs
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What is the reference for the separate mounting kit for LRD4369 overload relay
The LRD43xx type of thermal overload relays are directly mounted to the contactors LC1D115 & LC1D150 only. There is no separate mounting kit for the LRD43xx.
If a separate mounting is required for the contactors LC1D115 or LC1D150 type, then LRD336xx shall be selected as these range of overload relays have independent mounting and have similar setting ranges and are of Class 10A.
If a separate mounting is required for the contactors LC1D115 or LC1D150 type, then LRD336xx shall be selected as these range of overload relays have independent mounting and have similar setting ranges and are of Class 10A.
Released for:Schneider Electric Egypt and North East Africa
Explore more
Range:
Explore more
Range: