{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.

Is It essential to use the external neutral sensor TCE with Micro logic trip unit "6" for Masterpact ACB of types NT and NW ?

Kindly be informed that the external neutral sensor of type "TCE" is essential to be used with Masterpact ACB of types NT or NW in Micrologic trip unit "6" if the CB is of 3 poles

while it is not used if the NT or NW ACB is 4 poles

Schneider Electric Egypt and North East Africa