{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What is the function of the "Ap" led in micrologic ?
Kindly be informed that the Ap light of the micrologic indicates a number of errors on the micrologic trip unit such as excessive temperature or short-circuit higher than circuit-breaker capacity or internal fault inside the trip unit.Please refer to the attached page.

Thanks to verify the following:

1-Ambiant temperature around the breaker

2- Elimination of fault cause if any.

3- Press the reset Button and try to close the breaker.If the circuit breaker remains closed and the Ap LED remains on, contact the Schneider Electric after-sales support department.

Schneider Electric Egypt and North East Africa

Attachment(s)
Micrologic A,E fault indication.pdf [138.25 KB]