{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What version of Unity Pro will run on Windows 10?

Issue
At what release did Unity Pro begin supporting Windows 10?

Product line
Unity Pro, Control Expert

Resolution
Windows 10 OS support began with Unity Pro V11.0 which supports:
- Windows 7 32&64 bits
- Windows 8.1 32&64 bits
- Windows 10 32&64 bits
- Windows Server 2012

as of 7/1/2022 the latest Unity Pro version release has been renamed and is now EcoStruxure Control Expert V15.1 which supports:
-  Microsoft Windows 7 Professional edition 32/64 bits SP1
-  Microsoft Windows 10 32/64 bits
-  Microsoft Windows Server 2016
NOTE: An operating system Windows 64 bits is mandatory for projects with Modicon M580 controller, or projects using DTMs.
Unity Pro is now called EcoStruxure Control Expert starting at version14.0


Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: