{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can a variable be assigned to the ATV32 Somove timer function block?

Issue:
Assign a Timer Function Block on an ATV32

Product Line:
Altivar 32

Environment:
Somove function block for the ATV32 all serial number

Cause:
N/A

Resolution:
No, a variable cannot be assigned to the timer function of the ATV Logic, Timer function block properties.   The on and off delay time is hard set in the function block properties.

Schneider Electric Egypt and North East Africa