{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What could cause Hex error 3410 (Network module missing) on an M580 L9_MSTR function block?
The high byte or MSB of the 4th implied word in the control array for the M580 L9_MSTR function block must be set to 65,024 Dec  or 16#FE00 Hex in order for the block to communicate out from the M580 native ethernet port.

If the project was converted from Concept Software, and you are using the MBP_MSTR,  make sure that you are using a located 9 WORD array for the Control pin.  Concept allowed a single WORD there and Control Expert does not.

Schneider Electric Egypt and North East Africa