{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How to send an Explicit Message to the Ethernet IP device connected to the 140NOC78000
Issue
This resolution provides a demonstration on how to connect the 140NOC78000 and send an explicit message to the
Ethernet IP slave device.

Product Line
140NOC78000

Environment
Windows 7

Resolution
The attached video provides a demonstration on how to connect the 140NOC78000 and send an explicit message to the
Ethernet IP slave device using the DTM Ethernet IP Explicit Message tool that is included with Unity Pro..

Schneider Electric Egypt and North East Africa

Attachment(s)
How to send an Ethernet IP command to a slave attached tot he 140NOC78000.7z [1.02 MB]