undefined undefined
{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Does the PM5500 series meter support BACnet IP?

Issue
Customer is asking if PM5500 meter supports BACnet IP

Product Line
PM5560 (METSEPM5560)
PM5563 (METSEPM5563)

Environment
Firmware upgrade

Resolution
BACnet IP protocol is now available as a standard feature on all PM5500 series power meters. BACnet is an open, industry-standard protocol that allows data to be easily shared between devices from different manufacturers. Simultaneous communication via BACnet and Modbus over Ethernet allows more than one system to communicate with the same meter at the same time. PM5500 meters are BTL tested and approved to assure buyers and reduce the risk of integration errors and the associated costs in the field. Firmware in existing meters can be upgraded to version 2.3.0 to enable BACnet IP communications. For details on upgrading firmware on the PM5500 series, reference Video: PowerLogic PM5500 - Upgrade Procedure for Firmware using FTP | Schneider Electric USA


Firmware version 2.3.0 can be found in the above FA299853 or from the following link: PM5560 PM5563 V2.3.0 Firmware and associated files (Revision History, Register List, Whats New, MIB, etc.) | Schneider Electric

The updated documentation is linked below.
PowerLogic PM5000 Handout: https://www.se.com/us/en/download/document/4100BR1501R04/
PowerLogic PM5500 Series User Manual: https://www.se.com/us/en/download/document/HRB1684301/

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: