{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Will Vijeo Designer Runtime 6.2 run on Windows 10?
Issue:
Looking to confirm if Vijeo Designer Runtime 6.2 will run on Windows 10

Product Line:
Vijeo Designer V6.2

Resolution:
As of Vijeo Designer 6.2 SP6, all tests have been completed to certify that Vijeo Designer Runtime can run on Windows 10. When installing Vijeo Designer V6.2 (base version), ensure you right-click on the install.exe file and "Run As Administrator". This will ensure you have full privileges to install the software. Once you have installed the base version, apply any service pack SP6 or greater.

Schneider Electric Egypt and North East Africa