{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can I run a larger hp motor with a smaller hp softstarter ?
Issue:
Can I run a larger hp motor with a smaller hp softstarter

Product Line:
ATS48 , ATS22, ATS01

Environment:
All

Cause:
Need to up size the motor for application

Resolution;
No, it is not recommended using a smaller hp softstarter on a larger hp motor. The Softstart horsepower should match the motor and ampage should at higher than the motor rating.

Schneider Electric Egypt and North East Africa